Schneider Electric

Home | Contact





Product Specification Sheets

EcoStruxure™
Foxboro™ DCS
Click here for the latest preferred products for EcoStruxure™, Foxboro™ DCS, Foxboro Evo™, and I/A Series® - recommended for new system projects, system expansions, and system upgrades.
EcoStruxure™
Foxboro™ SCADA
Click here for EcoStruxure™ Foxboro™ SCADA products.
Foxboro Evo™ and I/A Series™ Available
Click here for available products - targeted at existing installation support.
Foxboro Evo™ and I/A Series™ Mature
Click here for mature products withdrawn from sale and for mature PSS numbers superseded by new PSS names for existing products.
FCS/InFusion™ Control System Lifetime
Click here for lifetime products - withdrawn from sale.
All
Click here for all preferred and available products.
Download CD Image
Click here to access the ISO image download page for the PSS CD .


 Application Data  Sheets
All
Click here for all Application Data Sheets.


 
Welcome to
Product Specification Sheets/Application Data Sheets

Here you can download an ISO file of the PSS CD image containing the PDF versions of the Product Specification Sheets and the Application Data Sheets.

   Download
PSS CD Image
To download the PSS CD image, right click here and select Save to Target. A GCS website account is required to access this link.

If you have not logged into the Global Customer Support website, you will be prompted to log in. In the resulting Save dialog box, indicate the location for the file download. Click Save.
Once downloaded, you can either mount the iso image on your computer as a virtual drive using a virtual drive application such as Virtual Clonedrive or you can create a CD/DVD from the iso file using a CD/DVD burning application such as Roxio creator, Nero, or CDBurnerXP.

Double click the mounted iso image or insert the CD/DVD to access the initial PSS screen. If Autoplay is disabled on the computer, double click index.htm at the root of the CD to access the PSS documents.


© Schneider Electric | Legal